This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5160: Reg Inductor change in LM5160DNTR design

Part Number: LM5160

Dear All,

One of my  customer working on LM5160DNTR for Isolated power supply application for below specs, inductor value used in webench design is about 428uH with about it is generating 15V and since 428uH is not available , my customer used available value in market which is 470uH with which we are getting 15.7V, request you to clarify on same.

I/P voltage: 40-60V

O/P voltage: 15V, Current: 200mA

Aravind.