Hello,
Datasheet is specifying 500us start-up delay from EN with a 1ms soft start time.
However, I am measuring almost reversed numbers, 1.1ms start delay and 500us SS from 10% to 90% of Vout or almost 1ms from Vo ramp start to after Vo settling
I noted that this is consistent with the waveforms from the datasheet at page 11.
Is the 500us start-up delay time form EN to be corrected?
Thank you
Cosmin P