This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24210: Charging 10-12 Ah battery

Part Number: BQ24210
Other Parts Discussed in Thread: BQ25570, BQ25504

Hi,

I have Solar panel 5V@1A , is bq24210 can be use as charger and power supply for out door GSM module and single cell LiON/LiPo battery 10-12 Ah ?

Thanks

Haim Rodrik 

  • Hi,
    I'll recommend taking a look at the BQ25570 or the BQ25504 which are our energy harvesting devices that also have integrated chargers. The BQ25570 has a regulated output while the BQ25504 output follows the battery voltage.
    Regards,
    Raheem