Other Parts Discussed in Thread: LM46002, LMR16020
Hi,
we use the LMR16030 with 12V to 48V input and adjustable 6V to about 42V output. We adjust the switching frequency using external switched resistors. All works fine, except the temperature at 2A output current is too high.
Any idea for a solution with lower Rdson? We are not sure about the compensation, which is internal in the LMR16030, but most times external for others. With our requirements the COMP-circuit is diificult to calculate...
Thanks a lot for any hint!
Volker