This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5160: Reg Suggestion on Multiple output isolated power supplies

Part Number: LM5160

Dear ALL,

one of my customer working on 48VDC and 230VAC/325VDC Airconditioner , they need suggestion on multiple output isolated power supplies, plese find attached specs.

request you to suggest suitable reference design which can be used for Airconditioner application as per specs else suggest suitable device/application notes to address the same.

For 48V - 15V, 200mA - we suggested with LM5160 device and customer is ok with it.48VDC and 230VAC.docx

Aravind.