Other Parts Discussed in Thread: LM5170, TIDA-01168, PMP4333
Hello,
Can I use this IS for creating 12S LiPo rapid charger with two operating modes:
- constant current from 12 to 30A set by MCU
- constant voltage from 40 to 54.6V set by MCU
Module should be powered by external 46-52V source (up to 60A available).
Preferably, buck-boost converter.
Please direct me on useful recourses with reference schematics with LM5170-Q1 in mind.
If this IC is unsuitable, can you recommend good alternative starting point?
We usually worked with 6S packs (24V) and options are widely available for that but switch to 12S looks like creates serious lack of useful info on web...
Thsank you