This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51220A: OCP reaction time

Part Number: TPS51220A


Hi Sir:

Datasheet does not provide OCP reaction time.

Pls provide data Thank you.

  • Hello Jerry,

    In an overcurrent condition, the current to the load exceeds the current to the output capacitor thus the output voltage tends to fall down..When output voltage becomes lower than 70% of the target voltage, the UVP is triggered and an internal UVP delay counter begins counting. After 1 ms, TPS51220A latches OFF both high-side and low-side MOSFETs.

    So UVP delay time is OCP reaction time. It is 1ms.

    best regards.