Dear E2E,
Any suitable solution can support 0.3Vout/0.2A converted from 3.3Vin whatever LDO or buck converter?
BR,
Jason
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Mark and Kevin,
The load current is not constant.
It is variety in 0.2A.
I have a TLV62080 EVM board on hand.
Assume using TLV431 as reference voltage as 1.24V, calculate the injection resistor based on feedback devider [178k(high side) and 39.2k (low side)].
And then, get around 37k injection resistor with 1.24V reference voltage.
But, I found that 0.3V output voltage will be changed by load current from 0.27V to 0.35V with 0.2A to 0A.
Does it cause by min duty cycle?
any switching device is more suitbale for this condition?
I would like to apply that EVM board to test it again.
BR,
Jason