This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
For TPS65132, I have one question to set the Vpos register bit5, to be compatible with other competitors, customer want to set 1 to bit5 of Reg 0x00, which is reserved and our datasheet suggest set 0.
So if we write 1 to this bit5, is there any problems?
Since bit7~5 is only read, so if write 1 to this bit, is it still keep 0 for those bit?
Thanks.