I bought the evaluation board of BQ25606 to do some tests about chip's performance.
I noticed that when I place a very large load (about 2-3 Ohms) on the board and power on the chip with 5V (while load is already connected) input the current does not reach the expected value (3.68V / RL) but is limited to about 500mA instead.
Therefore the Vsys voltage is keepen clamped much below its typical value.
When I power up the board without connected load, and connect the board afterwards the chip is able to deliver the calculated current.
My settings is:
D+, D- floating.
RILIM = the least possible value (about 160Ohm).
CE = HIGH (Disabled)
Am I doing something wrong?