Hi,
I am using TPS53355 in my design to generate 1.1 V from 12V , at 28A max.
Please clarify below points related to this:
1) For 250Khz switching frequency, the Webench suggests to use 330nH , but calculation using datasheet formula ( equation 8) gives about 430nH. Please let me know which value can be selected for better performance.
2) As per equation 8 of the datasheet, Inductor value is inversely proportional to current. So inductor value for large current will be smaller and smaller current will be larger. Whether inductor value selected at Imax will cause any performance degradation when current is lesser than that?
( For example, in above case, inductor value for 28A is 430nH. But for 16A, inductor value comes to be 750nH. But as per datasheet, we have to select 430nH, by considering Imax. Whether this inductor will cause any functional issues when current is 16A?)
Thanks in advance.
Regards,
Madhu.