Hello,
I am using bq34z100-g1 with an 8 cell LiFePO4 and first of all I want to do the learning cycle. I have donde the following steps:
1. Enable IT
2. Charge the pack to full.
3. Let it relax for 2 hours.
4. Discharge the pack to cell Termination Voltage (3000mV, equivalent to the pack being at 24V) and let it relax for 5 hours.
However the MaxError did not change to 5%, it is 3% and learned Status and Update Status is equal to 0x05.
Now I am repeating the cycle but I am afraid Max Error remains at 3%. What are the things I am not doing well?
Here you have the registers of the bq34z100-g1 in case they were useful.
Thankyou very much in advance for your answers,