Is there any one can help for me?
I have done two failed learning cycle with BQ20Z45, Max Error, Qmax and Update status do not update after charging. I found that VOK never set to 1, when I send IT enable(0021) or start charging.
1. My cell type is LG INR18650 B4 2600mAh, I use the chemical ID 0297, is that correct?
2. I follow below step to do the learning cycle, and stop learning when failed at step7. Please see my log data and gg file attached.
Step1: Program .senc file with correct chemical ID, correct data flash, cycle count and update status are 0, max error is100%.
Step2: Calibrate the battery pack.
Step3: Discharge the battery pack to empty with C/5 (voltage down to term).
Step4: Wait 5 hours.
Step5: Send IT enable command (0021) , Bits QEN is set and VOK is cleared.
Step6: Charge pack to full with C/2 until the taper current is reached and the FC bit is set.
Step7: Let it relax for 5 hours.(Qmax is not updated, Update status keeps 04, Max Error keeps 100%)
Step8: Discharge the pack down to term voltage with C/5.
Step9: Let it relax for 5 hours.