This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC28025: How to design UC28025 in only one output application ?

Part Number: UC28025


    UC28025 is with totem Pole Outputs. If the application only wnat to use one output OUTA and OUTB does not use, how to connect these two pin in the circuit?Thank you
    • Hello Jerry,
      For single ended designs (where the required maximum duty cycle is less than 50% ) you can use OUTA by itself.
      OUTB is unused but you can terminated with a 10k resistor to ground. This will prevent any parasitic oscillations on the output

      Regards
      John