This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61193-Q1: TPS6119x - external clock synchronization with phase shift

Part Number: TPS61193-Q1
Other Parts Discussed in Thread: TPS61193

 Hello Team,

is it possible to use two of TPS61193 with external clock synchronization (pin 6) and shift phase by 180 degree? (driving power stage)

Background is that this would reduce the load transient when not both LED drivers are switched on simultaneously.

By having 180 degree phase shift only one of the TPS61193 is switched on and the other off.

Do you think this is feasible?

Many Thanks

Josef