I´m looking behalf of our designer for Li-Ion charger IC (EVM kit) with follow specs:
- Part: Battery charger reference board (EVM kit)
- Topology: Switch-mode buck
- Battery chemistry: Li-Ion
- Number of series cells: 1
- Control interface: standalone
- Operating Vin: 12V, 1.25A (typ); 5V, 2.5A (min)
- Battery charge voltage: 4.2V (min/max)
- Charge current: 2.5A – 3A
May I ask you kindly to confirm if item code: BQ25606 is only/best choise or could we consider to use some other too?
If BQ25606 recommended, couple questions
- Charger IC input: connected to the output of wireless power receiver?
- How to connect D+ and D- pins when there is 5V – 12V unknown adaptor at the VBUS input?