Dear Sir,
My customer has question on using SN9039 with Intel Cherry Trail platform on IPC application: when the system power is down abnormally, SN9039's will have abnormal power sequence on buck6(V1P8A), buck3(V1P15) and buck5(VNN) and will cause system halted before cleaning CMOS on intel NUC. Is there any method to solve the system halted issue on modifying SN9039's power off sequence ?
CH1: +V1.8 CH2: _V1.15 CH3: VNN Ch4: 5V
Or can customer use VBATSENSE signal or other method to force system into cold off sequence when abnormal power down?
Best regards,
Gary Teng