This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Charging bipolar-supply batteries in situ

Other Parts Discussed in Thread: BQ24725A

I am designing a device that will have two 7.2-V Li-ion battery packs in series, arranged to produce bipolar supplies.  The series connection between the batteries is my PCB's ground.   The batteries cannot be removed for charging.  One battery pack will see a greater load than the other one, so they cannot be charged in series (with a 4-cell charger); I will use one charger IC for each battery pack.  Both batteries need to be charged at the same time, however.

So far the only method I've thought of to charge these batteries is to break the batteries' connection to each other and their connections to the loads during charging.  I would do that by running all of these wires to a multi-pin charger receptacle.  To actually operate the hardware, the user would insert a loop-back plug that would make all of the necessary connections between the batteries and the loads.  Oh yes, during run-time I also need to break the Vin and VSS connections between the charger ICs, and use a local VSS for each one.  

Cumbersome, wouldn't you agree?  Any better ideas?  Thanks...

  • "One battery pack will see a greater load than the other one" and "Both batteries need to be charged at the same time"
    It seems you have two batteries and two system load and share with same input source.
    In this case, you can use two battery chargers to charge battery and power up each system load.

    If the system don't have SMBus, please check bq246xx or bq2417x.
    If the system have SMBus, please check bq24725A.