Other Parts Discussed in Thread: BQEVSW, BQSTUDIO
Trying to evaluate the BQ27530 using the EV2300 and BQ27530EVM. But, getting communication errors.
I contacted the Ti Chat and they were unable to make progress, so suggested I post here.
I have tried using BQSTUDIO and the bqEVSW software. But neither is working. Initially I had trouble with the EV2300 drivers but, I believe they are now installed OK. I get the Windows BEEP when I plug and unplug the USB and Device Manager is no longer showing any issues.
The EVM is also attached on USB cable. But, I don't get a Windows BEEP when I plug/unplug the EVM.
I have tried with battery attached and power supply and the I2C between the EV2300 and the EVM.
The error I am getting is "No communication with EVM Gas Gauge could be established."
Per the suggestion in the dialog, I do have a battery attached. The battery has 3.7V. So, I believe the apply power comment has been satisfied.
Any suggestions?
Thanks