Part Number: LM5145
In the datasheet p24 and p16, the ILIM comparator is different. Which one is correct? From p24, I think this method is to limit the peak current, not valley current.
U_ILIM=ILIM×R_ILIM -U_Q2_on
When circuit is in overload situation, U_Q2_on will be higher, and U_ILIM will be lower. If the U_ILIM is lower than zero, then a hiccup happened. So the lowest point in ILIM is ILpeak×R_ILIM -U_Q2_on . So it is to limit the peak current, am I right? And can you give me some me some waveform test on the ILIM pin to help me to understand the function of this pin?
When the OCP happen, why the ramp voltage will be higher than before? I can not understand the waveform below better, can you explain it for me? Thanks a lot!