This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC29002: Application of UCC29002

Part Number: UCC29002

HI

My client wants to use the UCC29002 under the following load conditions
Would it be possible UCC29002 applies to the following specifications?
Can I get a schematic with UCC29002 in similar specifications?

OUTPUT : 12V/6.7A

OUTPUT : 48V/16.7A