Hi,
I have a question for LMR16006.
I would like to construct an inverting buck-boost circuit.
Can I use it under the following conditions?
Vin=17~24V
Vout=-20V
Iout=10mA
If Vin is 20 V or more, I think that Vout = -20 can be outputted,
I am worried whether Vout = -20 V can be output at Vin 17 V.
Best regards,
Watanabe