Other Parts Discussed in Thread: TPS65920
There's a special situation we need to add external 75kohm resistor on VBUS as below.
The only USB function required for this OMAP platform is to act as a USB-Device (connected to PC for data transfer.) In addition, we need to detect a non-USB accessory plug-in event by detecting VBUS voltage. (The pin is connected to a big PU resistor to 5V on the accessory board.) Therefore, we need to add a 75kohm PD resisotr @ VBUS pin on this OMAP platform.
The question would be, is there any side effect to add 75kohm considering only USB-Device mode is required?
Antony