Other Parts Discussed in Thread: LAUNCHXL-TMS57004, EM1402EVM
Hello.
We are using BQ76PL455A-Q1 (IC,not EVM) for monitoring and passive balancing of 14 cells. The circuit connections have been made as mentioned in the typical application of the datasheet. We wanted to know if there were any checkpoints on the IC that we could check and ascertain that all the required connections for the IC have been made by us.
For example:- voltages across pins V5VAO,VM,VREF,VDIG etc. After the 14 cells (to be monitored) are connected, will these pins show output even if the host controller is not connected. If yes, what voltages do they ideally have to show, if all connections were made correctly.
If not, are there any others pins that can indicate correct connections to IC.