This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55332-Q1: convert 1.6V to 5V with using external bias

Guru 29720 points
Part Number: TPS55332-Q1


Hi Team,

Is it possible to configure the following schematic for TPS55332-Q1? 

- Vsupply: 1.6V
- Vout: 5V
- external bias: 5V (low power consumption)


The recommended operating conditions of TPS55332-Q1 shows VIN=3.6V~ however my customer wants to convert 1.6V to 5V with using external bias (5V).

Best Regards,
Yaita / Japan disty