Tool/software: WEBENCH® Design Tools
Hi,
Is there a way to force Webbench to simulate using 600Khz instead of 1.6Mhz, when using the LM2733?
I would like to convert 3.5V -> 35V @ 20mA load. I think Webbench always simulates with 1.6MHz since it complains that the max DC is 89%.
With 70% efficiency I would expect a DC of ~93%. This is just within the spec over the whole Temp. range, expected Ambient temp. range is <= 40dC.
Thanks