Hi
I have used LMZ31506 to power up the core voltage (1V0) for Artix 7 FPGA. And the ripple requirement is ± 30 mV.
Will it serve the purpose?
Regards
Jay
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Jay,
according to the datasheet it should not be a problem (see datasheet page 9-11).
Here for example you can see the graph from the datasheet for the output ripple for PVIN=VIN=5V and various output voltages.
With a proper layout you should be able to perform even better than 30mVpp output ripple.
Michael