This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS24720: Load output

Part Number: TPS24720


 When I use TPS24720 full load,there will be ladder up the phenomenon with the output 12V,38A.

  • Go to www.ti.com/hotswap and download the design calculator tool. Looks like you have something set wrong. Are you 100% sure that you are not powering up into a high load? If you are, use the PG signal to allow downstream load turn on after Vout has risen to full value.

    Brian