Soft start time equation is the below in datasheet,
Tss(ms) = (Css * 0.765 * 0.86) / 6u
When Css is 8200pF, I think Tss is 0.000899(ms). Is this correct although this is 899ns?
I think Tss(ms) is mistake, and Tss(s) is correct. Tss becomes 899us if my idea is correct.
But I think soft start time is about 1.5ms on datasheet Fig, 28 and 29. Is the equation of datasheet correct?
Best Regards,
Kohei Sasaki