This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51610: Is TPS51610 suitable for the Ice lake platform?

Part Number: TPS51610
Other Parts Discussed in Thread: TPS53659, TPS53622

Dear all,

customer need following parts for their Ice lake platform power supply, their requirement is following:

1. Has VID function, the voltage can be set as 0/1.1/1.6/1.8V;

2.16A continuous output current and 34A OCP current;

3. input voltage is 6~14V;

If TPS51610 is not suitable, could you please give me your recommendation?

Thanks.

  • Hi John,

    The TPS51610 is not suitable for Ice Lake designs. It's SVID bus was designed to support IMVP6 processors, not VR13. VID step size, IMON tolerances, and power state behavior, among other things could all be different and affect performance.

    For Ice Lake applications the the current range you're looking for I would recommend looking at the TPS53622 and TPS53659.

    Please let me know if you have any questions.

    Thanks,

    Carmen