Looking for a recommendation on 12V-12V DC-DC UPS with 2-cell Li-Ion batteries.
Output current will be 1-2A.
I have looked at BQ24133. Just wanted to check if it is correct and if there are better alternatives.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Looking for a recommendation on 12V-12V DC-DC UPS with 2-cell Li-Ion batteries.
Output current will be 1-2A.
I have looked at BQ24133. Just wanted to check if it is correct and if there are better alternatives.
Hi Vineet,
Can you explain a little bit more on the application for this battery charger?
For your application you want the output of the DC/DC converter to be the same as the input using a 2 cell battery? This would require the input to buck down to a 2 cell li-ion battery and then boost the battery voltage up to 12V again, this way, if there is any transient on the input, it will not be reflected on the output, as the boost converter is a separate system from the charger (the output will always be 12V regardless of input voltage or battery voltage). The input of the boost converter will have to be connected on the same net as the battery voltage.
In any case, if you are looking to buck down from a 12V input to charge a 2 cell battery, then bq24133 is the right choice for 2A charging.
How much does the input voltage vary? Since this is a buck converter, input voltage should not go any lower than ~8.8V to maintain a good margin for duty cycle at about 95% (8.4V max battery voltage output for the buck converter).
Regards,
Steven