Other Parts Discussed in Thread: CSD25404Q3
Dear sir,
I'm now designing a 1S power bank with BQ25703A. Here is my test result under output 5V/9V/12V:
Vin Iin Vout Iout efficiency note
3.988 1.48 5.16 1 87.42%
3.948 2.94 5.12 2 88.22%
3.906 4.39 5.01 3 87.65%
3.955 2.71 8.95 1 83.50%
3.884 5.24 8.57 2 84.22% with fan
3.95 6.32 8.4 2.5 84.12% with fan
3.93 7.23 7.89 3 83.30% with fan
3.927 3.72 11.85 1 81.12%
3.888 5.48 11.6 1.5 81.67% with fan
3.93 7.08 10.78 2 77.49% output is not stable
In order to get better system efficiency, I have some questions:
1. Can the loop partameter be re-optimised for 5V/9V/12V@1S application?
2. Can the switch frequency chang to below 800Khz?
3. The voltage drop on current sense resistor and BAT MOSFET is more than 0.1V. It may cause more than 3% efficiency loss for 1S application. Can the resistor be reduced and the CSD25402 be replaced by other MOSFET with lower DCR?
4. CSD25402 allows max 10A current. Is there any other MOSFET with higher current can be used? My target is to support 30W output power for 12V.
Thanks
BR
Ren