This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A91: Circuit design review

Part Number: TPS7A91


Hello

One of my clients is using the TPS7A91 for this project.

It seems to me that it was applied with the right design values.

Could you please take one more review?

I will deliver the corresponding schematic file.

<<schematic deleted>>

  • Hi Kim,

    The values and configurations seem to be reasonable. The only comment I would add is that if greater accuracy is required, take into account the output voltage offset contribution resulting from the feedback pin current and use 0.1%-tolerance resistors instead of 1%-tolerance.

    Regards,
    Jason Song