Hi
There are some unused pins on the customer setting.
That are VCC3 and VCC6. (LDO1 and LDO2, LDO6 and LDO7 and LDO8)
I have some question in that case as below.
1.How can we configure VCC3 and LDO6~LDO8 if we do not use VCC3?
VCC3 can be connected to gournd if it is unused? LDO6~LDO8 can be left open?
2.How can we configure VCC6 and LDO1~LDO2 if we do not use VCC6?
VCC6 can be connected to ground if it is unused? LDO1~LDO2 can be left open?
3.How do NRESPWRON work if we do not used VCC3 and VCC6?
Do NRESPWRON ignore the LDO1 and LDO2, LDO6~LDO8?
Please give us how we should set those pins if those pins are unused.
Regards,
Koji Hamamoto