This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZ31704: Circuit design review

Part Number: LMZ31704


Hello

One of my clients is using the LMZ31704 for this project.

It seems to me that it was applied with the right design values.

Could you please take one more review?

I will deliver the corresponding schematic file.

<<schematic deleted[LE]>>

  • There are a couple of things that need to be corrected in these schematics.
    - R76 & R52 need to be changed to 1000kΩ (1MΩ).
    - A ground connection is required between R49 & R52.
    - For all 3 schematics, a capacitor should be placed on SS/TR and a resitor should be placed on OCP_SEL