This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92692-Q1: spread spectrum frequency

Guru 20090 points
Part Number: TPS92692-Q1


Hello,

Are there any recommended spread spectrum frequency?
From the datasheet,  is the 100 Hz to 1.2 kHz ?
I would like to know the rule of thumb for deciding spread spectrum frequency.

Best Regards,
Ryuji

  • Hello Ryuji-san,

    There isn't really any sort of rule. The range given is in case certain frequencies in that range may not be desirable in a system mostly. The most common practice is to set it in the middle around 600Hz and that is typically fine for most applications. But it can be changed if the EMI results need to be adjusted some.

    Regards,

    Clint