This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R1: Under Temperature Behavior Clarification

Part Number: BQ40Z50-R1
Other Parts Discussed in Thread: BQ40Z50-R2

Hi folks - 

I'm using TS1 & TS2 thermistors to report Cell Temperature and configured to report maximum of it. (TS3 & TS4 are unused and connected to Vss as suggested in the data sheet). 

Settings

Configuration

Temperature Mode

0

hex

Settings

Configuration

DA Configuration

15

hex

 

We understand for overtemperature protection, reporting the maximum of TS1/TS2 works fine. It will detect over-temperature condition based on maximum of two.

But for under temperature, will it still see maximum of TS1 & TS2 to detect under temperature?  Will it report the maximum of them or minimum of them?

We wanted to have worst out of two thermistors for over temperature as well as for under temperature detection.

Do you have any advice for this use case?  

Will this behavior be the same for BQ40Z50-R2? 

Thanks,
Jake