This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61500: TPS61500 Min. PWM freq.

Part Number: TPS61500

We are using the TPS61500 as a LED driver for IR illumination.
The circuit drives 4 LEDs at a 2.2A synchronized with the camera shutter.
It's straight out of the datasheet. Input voltage is 12v, pulse time is 2ms.
LED combined forward voltage is ~13.5v

When the frame rate is > 50 fps the circuit works fine. At somewhere
around 47 fps the current suddenly falls to around 1A.

I have  tried different values for the soft start cap, the input caps, the output caps
and the freq resistor. I have also tried removing the soft start cap altogether, all of
this to no avail. Always at around the same 47Hz frequency, the output current suddenly
drops. 

What causes this sudden drop ? Is there any way around it ?

Our new cameras run at 20 fps so I need to find a solution.

Thanks,
Yaacov