This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3281: Powering directly to the output side

Part Number: LM3281


I'm using a third party module in my design which includes a TI LM3281 to regulate from 5V to 3.3V DC.

That part of schematic is straightforward, shown below:

The module vendor seems to imply we can supply the module directly to the 3.3V net from a pin directly connected to VDD33 above.

However there is some confusion if this is possible or not and some users apparently already damaged the module for operating it like that (regulated 3.3v supply to VDD33, while +5V  input floating) but it works fine for others. It does seem bad practice at the very least.

Is it true operating the circuit by feeding an externally regulated 3.3V into VDD33 while Mode, EN and Vin are floating can damage this circuit?

If it does cause problems can you suggest a solution to enable powering it safely from either ~ 5V or externally regulated 3.3V? Keeping current consumption as low as possible is extremely important, hence why we'd like to power from the 3.3V pin and avoid the bypass mode.

I know removing R10 zero ohm resistor would be the best option  but this is an educational system so asking users to solder/desolder SMD resistors depending on how they power it is not possible.

Thank you

  • Yes it is a bad idea to power any regulator from it's output.  There is a parasitic diode from input to the switch pin

    that will be turned on in this configuration and can cause damage.

    The easiest way to power from two supplies would be to use a simple diode-OR connection. 

    However, this will cause a voltage drop in your supply rail due too the diode drop.

    You might also look at some of TI's "ORing" controllers such as the LM5050 or similar.