This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP87524B-Q1: Any options for modifying OTP

Part Number: LP87524B-Q1

I think listing OTP/EPROM as a feature of the LP87524B-Q1 is misleading.  It seems there is no way to program it, even once!

I understand it is programmed once at the factory, but I can't find any way to program it on my board.  If the user can't program it, you should label it ROM.

I designed the part in to my board assuming (incorrectly) I could program it.  Now I am stuck.  The default values for Boost2 and Boost3 are too high and will damage components.  My plan was to power the board with the regulators disabled and program the OTP from external I2C as part of the first time board bring up.  It's a little inconvenient, but the other features of the LP87524B-Q1 made it worth the hassle.  Powering up disabled and programming over external I2C works fine, but I can't do that in the application.  There is nothing to power then on-board I2C until Boost0 is active.

It wasn't till I was testing the new boards today that I realized there are no instructions in the data-sheet for programming the OTP.  My fault for not doing better research, but I could sure use some help if there are any other options.  I am even considering Zeners on Boost2 and 3 to protect my components and trip over current shutdown on those rails to give me a chance to re-program them after power up.

Any other ideas?

  • Hi Barry,

    As you already realized, OTP (One Time Programmable) memory can be programmed only once and it is done in manufacturing. If you would like to have custom OTP configuration programmed for you, please contact your local TI sales representative.

    Regards,
    Juha