Hi,
I am having some troubles with the PTC function.
When activating the PTC function and heating it up to 200c it will not disconnect the DSG&CHG fets (The PTCEN pin short to BAT and PTC type used same as in the application schematic).
The commands I send to activate it are:
PF_EN=1
Settings - Permanent Failure - Enabled PF C - PTC=1
After configure the above and sending a RESET command, the PF flag in Operation Status A is set and DSG&CHG fets are disconnected (XCHG&XDSG=1).
I don't understand what I'm doing wrong.
Appreciate your help.