Hi
We are referring table 2 from datasheet.
The requirement is following.
IN:11V - 26.4V
OUT : 10V / 0.4A
Fsw = 1000KHz
We are about to take parameter from table 2 at Fs = 1000KHz and Vout = 12V, then L = 6.8 uH is selected.
According to the Figure 2 of datasheet, L = 6.8uH could be selected even if Vin and Iout is varied.
Is it OK to take parameters from table 2 for our requirement?
BestRegards