This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR16006: To much EMC noise

Part Number: LMR16006


Hi Texas!

I have used LMR16006Y to supply 15V ~0.2A, with 36V input voltage, but it seams to emits more noise than accepted by EN55011.
First I though that the noise was due to my "bad layout", so I changed my layout according to App notes,
but it still emits to much noise.
I have tested TI's evaluation board with 18V input battery and 5V output, and 50R load.

The EMC noise from the Evaluation board is about 20dB too high!

What can I do? can anyone give me an alternative to LMR16006, the input voltage is 36V but must tolerate 50V