This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq24650 maximum input

Other Parts Discussed in Thread: BQ24650

From: Pardee, Sarah
Sent: Monday, August 30, 2010 2:05 PM

 

My customer, really needs to work up to and include 32V on the BQ24650.  The ABS MAX is rated at 33V.  He plans on clamping the input at 32.1VDC (should never see more than 32VDC for extended periods) is this OK?