Hello,
I am working on a project an LED driver with the following spec -
1. Universal Input, 85-265Vac
2. O/p current of 1.2A, Analog standard 0-10V dimming
3. 45-65 Hz freq range
4. Output OV threshold of 26 to 30V, o/p overcurrent threshold of 1.3-1.5 A.
I see that the UCC28810 fits my requirements however I am not certain that the OV thresholds could be met. Is there any other IC you would recommend ? Or would a design change be possible.
Is any IC which has an opto couple integrated into the chip for sensing output current?