I want to a platform over the USB OTG connection using both a PC that enumerates and a dedicated USB charger that does not enumerate. The PC enumerate to a 500mA supply and the current limit of 4030 is set appropriately. The dedicated USB charger does not enumerate and therefore does not set the current limit of the 4030.
Does the 4030 automatically detect the presence of a dedicated USB charger? If so how and what register can be read to determine that a dedicated USB charger is connected? Or is there a need for software control to determine the presence of a dedicated USB charger?