Hello,
Two kinds of package information are listed in the data sheet.
One of the YZP(R-XBGA-N8) in P21, Another of YZP008 in PACKAGE OUTLINE.
Which is correct YZP (R-XBGA-N8) or YZP008?
Regards
Taichi Nakamura
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Taichi,
The only difference between these two packatge drawings is the dimensions of D and E, and these will not change the recommended layout or footprint for the device. If outer dimensions are required, please use the information on page 21. I will work with our team to get this corrected.
Thanks,
Alek Kaknevicius