This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65911: PWRDN configuration

Part Number: TPS65911

Hi

>The PWRDN input is a reset input with selectable polarity (PWRDN_POL). High(low) level at input forces the TPS65911x device into off mode, causing a power-off reset. 

Does it put into Off-mode if PWRDN is low? I do not understand the above explanation ("High(Low) level at input forces the TPS65911x device into off mode")

Is the following my understanding correct?

 - High (supplied from VRTC) ; normal (operation) mode

 - Low (connected to GND) ; Off mode

Also should we use the pull up resistor when it is connected to VRTC?

Regards,

Koji Hamamoto