Other Parts Discussed in Thread: TPS62743
hi all
now my customer wants a device : 300mA DCDC (5V --> 3.3V) +100mA LDO(3.3V --->1.8V)
and I find TPS54120 is OK but the package is too large. Do we have much smaller package than TPS54120.
because they have another choice the competitor is only 1.2mm x 1.6mm.
thanks a lot