This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5175-Q1: SS programming

Part Number: LM5175-Q1


Hoi TI supporters,

I have questions about the LM5175-q1.

For a project of my school, I would like to use LM5175-q1 to convert the input voltage (9 - 30 Volt DC) to 12 Volt DC for the fan. But there is a probleem with the inrush current of the fan. The used fan need 3,42 Ampere for the inrush curren.

There is the SS programming which is integrated in de chip. So my question is can I use it for the fan which has the inrush current of 3,42 A?

The nominaal voltage of the fan is 12 V

The nominaal current is 0,66 A.

Power 7,3 W.

Best regards,

Hao Tran